Wählen Sie ein anderes Land oder eine andere Region, um Inhalte für ihren Standort zu sehen
Virtual trade show | Machine tool

TNC7: innovative, sustainable, and dependable

Further developed to include four hardware variants and new done-in-one machining capabilities, the TNC7 continues to raise the benchmark for intuitive CNC operation and reliable shopfloor processes.

Discover intelligent and innovative solutions for agile and efficient manufacturing!

Empower manufacturing:
Intelligent system solutions for machine tools and automated manufacturing processes

Discover exceptional accuracy, reliability, and performance through carefully engineered systems 
and perfectly matched components from the HEIDENHAIN CORPORATE GROUP. 
As a partner, we support you in achieving efficient, agile, and resilient manufacturing processes.

New technologies for the TNC7

In the future, the 19-inch and 24-inch variants of the TNC7 will offer cylindrical grinding and shaping operations. These functions will round out the TNC7’s machining capabilities while further enhancing the dimensional accuracy, contour fidelity and surface quality of workpieces. Single-setup machining with milling, turning and grinding operations will be easier than ever for TNC7 users.

The TNC7 and TNC7 basic will also offer new cylinder surface machining capabilities. In addition, new simulation and graphical programming functions are making TNC7 controls even more intuitive to operate through improved user guidance and new analysis options.

Automation solutions for more
agile and efficient manufacturing

The OC 310 multi-functional override controller

Two potentiometers in one multi-functional operating element: the new OC 310 override controller facilitates working with a TNC7, since the user can now regulate both the feed rate and rapid traverse with just this one operating element. The user is supported by the new “Conditional stop” software function, for intuitive, convenient and one-handed proving-out of NC programs. The user simply defines breakpoints in the NC program at which the control will stop during program run (such as before a tilting function, when the tool is changed, or when the machining feed rate changes to rapid traverse). The override controller vibrates to generate tactile feedback, simplifying the user's workday. Each user can define the events for which this function is active.